uKonn-X is the first seamless, digitally and visually supported system with bidirectional communication between design, development, assembly and commissioning. Classic wiring of machines through control cabinets and terminal strips is outdated. Decentralization can generate significant efficiency benefits. We connect the physical with the digital world. The goal is the holistic optimization of electrical installation technology – from planning over commissioning, all the way to maintenance.
To achieve this goal, we have developed uKonn-X. uKonn-X is a system that addresses all interfaces with electrical automation technology products as a digital solution. The focus of our digital solution is the seamless connection of all participants - human and product - along the entire product development process. In the first expansion stage, uKonn-X works as follows:
Step-by-step
Why uKonn-X?
Features
Step-by-step visualizations
The users receive a visualization of the current installation step to simplify the electrical installation. After identifying a cable, the complementary installation instructions are displayed. This avoids confusion and oversights.
Unique identification
The components used during the electrical installation can be marked with machine-readable codes, if required. This enables unique identification using a mobile end device (scanner, smartphone or similar).
Needs-based guidance
uKonn-X supports the user at the respective point of installation specifically with the required information.
Checklists for assembly plans
The entire electrical installation process is clearly displayed in the application. This allows the work progress to be viewed in real time and the assembly to be processed sequentially.
Digital documentation
Changes can be directly entered and approved in the system and are subsequentially stored in the database - completely paperless.
Task-specific display formats
uKonn-X enables the import of CAD files, topology and circuit diagram, so that those involved can switch flexibly between the desired illustration of the desired information.
Seamless communication
If changes to the electrical installation are necessary, the operator can conveniently communicate these digitally to the design department via an integrated function. Starting from the installation, this supports the development, improves the design of the machine and at the same time ensures accurate documentation.
Across departments and processes
The steps of the entire product development process are seamlessly and smoothly connected - Seamless Electrical Installation. Assign individual user roles and authorisations to provide your employees with exactly the information that is relevant to them. Facilitate cross-functional exchange and increase transparency in your operation.
Mobile und integrative
uKonn-X can be used on various end devices and supports the integration of scanners, external test devices and smartphones.
Components
Software
The uKonn-X software is an interactive application that visualizes individual assembly steps - exactly where they are needed.
Compatible with: Tablet, laptop, PC, mobile devices
Hardware
uKonn-X interacts with external hardware such as mobile scanners. This enables clear and unique identification of relevant cables and modules.
Process data
Get an overview with clearly prepared process data to identify training needs, optimisation potential and changes to your machine.
Request an appointment now!
If you would like to make an appointment to see uKonn-X, please fill in the form and we will contact you to arrange a meeting.
You also can apply as a pilot user to be able to accompany an exciting product from the very beginning. We can improve a product together and you can influence it. For this purpose, please tick the checkbox in the form below.